SLVSHP8A January 2026 – June 2026 TPS544B28
PRODUCTION DATA
The device monitors a resistor-divided feedback voltage to detect overvoltage and undervoltage events. The OVP function enables when the output is enabled. The UVP function enables after the soft-start period is complete.
After soft-start is complete, if the FB voltage becomes lower than 85% of the VREF voltage, the UVP comparator trips and an internal UVP delay counter begins counting. After the 70µs UVP delay time, depending on the selected fault recovery mode in (45h) VOUT_UV_FAULT_RESPONSE, the device either hiccups and re-starts after a sleep time of 56ms or latches off both high-side and low-side MOSFETs. The latch-off fault can be cleared with a reset of VIN or by toggling the EN pin. When a UVP fault occurs, the VF bit in (79h) STATUS_WORD is set and can be cleared with (03h) CLEAR_FAULTS.
When the output is enabled, the FB voltage must rise above the 90% PG low-to-high threshold to clear the UVP comparator. If the FB voltage does not exceed the 90% threshold by the end of the soft-start period, the device responds to the undervoltage event.
During the UVP delay time, if the FB voltage becomes higher than the 90% PG low-to-high threshold, the undervoltage event is cleared and the timer is reset to zero. When the output voltage falls below the 85% UVP threshold again, the 70-μs timer re-starts.
When the FB voltage becomes higher than 110% of the VREF voltage, the OVP comparator trips and the circuit latches the fault condition and drives the PG pin low. The high-side MOSFET turns off and the low-side MOSFET turns on until reaching a negative current limit INOCL. Upon reaching the negative current limit, the low-side MOSFET is turned off, and the high-side MOSFET is turned on again, for a proper on-time (determined by VO/VIN/fSW). The device operates in this mode until the output voltage is pulled down under the UVP threshold. The device then responds to the undervoltage event responds as defined in (41h) VOUT_OV_FAULT_RESPONSE. When an OVP fault occurs, both the OVF bit in (78h) STATUS_BYTE and the VF bit in (79h) STATUS_WORD are set and can be cleared with (03h) CLEAR_FAULTS.
If there is an overvoltage condition prior to the output being enabled (such as a high prebiased output), the device responds to the overvoltage event as described above at the beginning of the soft-start period. The device waits until the completion of the soft-start period for UVP to be enabled, and depending on the selected fault recovery mode, the device either hiccups and re-starts after a sleep time of 56ms or latches off .
When the fault response is set through pinstrap, the fault response is identical for both OVP and UVP. However, if different responses are desired, the responses can be set independently through (41h) VOUT_OV_FAULT_RESPONSE and (45h) VOUT_UV_FAULT_RESPONSEAs an additional layer of protection, the device implements a fixed OVP that, unlike the percentage-based OVP, is active even before soft-start is complete. The fixed OVP thresholds are determined by (29h) VOUT_SCALE_LOOP and can be enabled/disabled in (D1h) SYS_CFG_USER1. The fixed OVP thresholds are defined in Table 7-11.
| VOUT_SCALE_LOOP (V/V) | FIXED OVP THRESHOLD (V) |
|---|---|
| 1 | 1.1 |
| 0.5 | 2.2 |
| 0.25 | 4.4 |
| 0.125 | 6.6 |