SLVSI22 August   2025 DRV8844A

PRODUCTION DATA  

  1.   1
  2. 1 Features
  3. 2 Applications
  4. 3 Description
  5. 4 Pin Configuration and Functions
  6. 5 Specifications
    1. 5.1 Absolute Maximum Ratings
    2. 5.2 ESD Ratings
    3. 5.3 Recommended Operating Conditions
    4. 5.4 Thermal Information
    5. 5.5 Electrical Characteristics
    6. 5.6 Switching Characteristics
  7. 6 Detailed Description
    1. 6.1 Overview
    2. 6.2 Functional Block Diagram
    3. 6.3 Feature Description
      1. 6.3.1 Output Stage
      2. 6.3.2 Logic Inputs
      3. 6.3.3 Bridge Control
      4. 6.3.4 Charge Pump
      5. 6.3.5 Protection Circuits
        1. 6.3.5.1 Overcurrent Protection (OCP)
        2. 6.3.5.2 Thermal Shutdown (TSD)
        3. 6.3.5.3 Undervoltage Lockout (UVLO)
      6. 6.3.6 CLR_FAULT and nSLEEP Operation
  8. 7 Application and Implementation
    1. 7.1 Application Information
    2. 7.2 Application Information
      1. 7.2.1 Driving Solenoid Loads
      2. 7.2.2 Driving Stepper Motor
      3. 7.2.3 Driving Brushed DC motor
    3. 7.3 Power Supply Recommendations
      1. 7.3.1 Bulk Capacitance
    4. 7.4 Layout
      1. 7.4.1 Layout Guidelines
      2. 7.4.2 Layout Example
      3. 7.4.3 Thermal Considerations
        1. 7.4.3.1 Heatsinking
      4. 7.4.4 Power Dissipation
  9. 8 Device and Documentation Support
    1. 8.1 Documentation Support
      1. 8.1.1 Related Documentation
    2. 8.2 Community Resources
    3. 8.3 Support Resources
    4. 8.4 Trademarks
    5. 8.5 Electrostatic Discharge Caution
    6. 8.6 Glossary
  10. 9 Revision History
  11. 10Mechanical, Packaging, and Orderable Information

Bulk Capacitance

Appropriate local bulk capacitance is an important factor in motor drive system design. Having more bulk capacitance is generally beneficial, although the disadvantages include increased cost and physical size. Bulk capacitors near the motor driver act as a local reservoir of electrical charge to smooth out the motor current variation.

Experienced engineers often use general guidelines about bulk capacitance to select the capacitor values. One such guideline says to use at least 1 to 4μF of capacitance for each Watt of motor power. For example, a motor which draws 2 Amps from a 24V supply has a power of 48 Watts, leading to bulk capacitance of 48 to 192μF, using this general guideline.

The voltage rating for bulk capacitors must be higher than the operating voltage, to provide margin for cases when the motor transfers energy to the supply.

A large value of bulk capacitance is desired to provide a constant motor supply voltage during current transitions, such as motor start-up, changes in load torque, or PWM operation. A working estimate of the required capacitance for consistent supply is essential to reduce complexity, cost and size of board electronics. We can use a general guideline method to find an appropriate capacitor size based on the expected load current variation and allowable motor supply voltage variation:

Equation 4. C B U L K > k   ×   ∆ I M O T O R × T P W M / ∆ V S U P P L Y

Where:

CBULK is the bulk capacitance

k is a scale factor to account for the ESR for typical capacitors in this type of application; based on the lab measurements with DRV8718-Q1EVM, k ≈ 3 is practical for these cases.

ΔIMOTOR is the expected variation in motor current, imax – imin

TPWM is the PWM period which is the reciprocal of the PWM frequency

ΔVSUPPLY is the allowable variation in the motor supply voltage

Figure 7-7 plots several data points and applies this general guideline, showing relatively good agreement.

DRV8844A Measured Results and 3x
                    General Guideline, Accounting for Real-World Non-Zero ESR Values of Electrolytic
                    Capacitors Figure 7-7 Measured Results and 3x General Guideline, Accounting for Real-World Non-Zero ESR Values of Electrolytic Capacitors

For more information please see the Application Note Bulk Capacitor Sizing for DC Motor Drive Applications .