SLVSM19 July 2026 TCAN942H-Q1
ADVANCE INFORMATION
The TCAN942H-Q1 is designed to be passive to the CAN bus if the device is unpowered. The bus pins were designed to have low leakage currents when the device is unpowered, so the pins do not load the bus. This is critical if some nodes of the network are unpowered while the rest of the network remains operational.
The logic pins also have low leakage currents when the device is unpowered so that the pins do not load other powered circuits.