SLVUCJ6 November 2022 LP5890
The LP5890EVM can be cascaded in a daisy chain. In such case, each LP5890 works in the independent mode (compared to the stackable mode). The host MSP430F5529 LaunchPad sends the serial data to the first LP5890 through the 40-pin BoosterPack Header. Then the first LP5890 transmits the serial data through board-to-board connector (J3 and J4) to the second LP5890. The second LP5890 can transmit the serial data to the host with an additional 1-pin cable. The serial data are transmitted through the daisy chain, while the clock signal is shared between multiple devices.
When multiple LP5890EVM are cascaded in a daisy chain, using an external power supply is recommended due to the large current consumption. Also, an additional digital buffer for SCLK may be needed if the drive strength of the controller is not enough.
Dual cascaded LP5890EVM in independent mode can be quickly set up and tested by following these steps:
Connect the J4 connector of the first LP5890EVM to the J3 connector of the second LP5890EVM. The direction is shown in Figure 3-3.
(Optional) Connect the SOUT pin of connector J2 on the second LP5890EVM to the P3.1 pin of connector J4 on the MSP430F5529 LaunchPad through an additional 1-pin cable that is marked as the bottom blue line in Figure 3-3. This step enables LP5890EVM to report LOD (LED Open Detection), and LSD (LED Short Detection) out to the host MSP430F5529 LaunchPad.