SLVUCR8A September   2023  – March 2024 TPS25751

 

  1.   1
  2.   Read This First
    1.     Notational Conventions
    2.     Glossary
    3.     Related Documents
    4.     Support Resources
    5.     Trademarks
  3. 1Introduction
    1. 1.1 Introduction
      1. 1.1.1 Purpose and Scope
    2. 1.2 PD Controller Host Interface Description
      1. 1.2.1 Overview
      2. 1.2.2 Register and Field Notation
    3. 1.3 Unique Address Interface
      1. 1.3.1 Unique Address Interface Protocol
  4. 2PD Controller Policy Modes
    1. 2.1 Overview
    2. 2.2 Source Policy Mode
    3. 2.3 Sink Policy Mode
  5. 3TPS25751 Registers
  6. 44CC Task Detailed Descriptions
    1. 4.1 CPU Control Tasks
      1. 4.1.1 'Gaid' - Return to Normal Operation
      2. 4.1.2 'GAID' - Cold Reset Request
    2. 4.2 PD Message Tasks
      1. 4.2.1 'SWSk' - PD PR_Swap to Sink
      2. 4.2.2 'SWSr' - PD PR_Swap to Source
      3. 4.2.3 'SWDF' - PD DR_Swap to DFP
      4. 4.2.4 'SWUF' - PD DR_Swap to UFP
      5. 4.2.5 'GSkC' - PD Get Sink Capabilities
      6. 4.2.6 'GSrC' - PD Get Source Capabilities
      7. 4.2.7 'GPPI' - PD Get Port Partner Information
      8. 4.2.8 'SSrC' - PD Send Source Capabilities
      9. 4.2.9 'MBRd' - Message Buffer Read
    3. 4.3 Patch Bundle Update Tasks
      1. 4.3.1 'PBMs' - Start Patch Burst Mode Download Sequence
      2. 4.3.2 'PBMc' - Patch Burst Mode Download Complete
      3. 4.3.3 'PBMe' - End Patch Burst Mode Download Sequence
      4. 4.3.4 'GO2P' - Go to Patch Mode
    4. 4.4 System Tasks
      1. 4.4.1 'DBfg' - Clear Dead Battery Flag
      2. 4.4.2 'I2Cr' - I2C Read Transaction
      3. 4.4.3 'I2Cw' - I2C Write Transaction
  7. 5User Reference
    1. 5.1 PD Controller Application Customization
    2. 5.2 Loading a Patch Bundle
    3. 5.3 GPIO Events
    4. 5.4 AUTO_NEGOTIATE_SINK Register
      1. 5.4.1 AUTO_NEGOTIATE_SINK Usage Example 1
      2. 5.4.2 AUTO_NEGOTIATE_SINK Usage Example 2
      3. 5.4.3 AUTO_NEGOTIATE_SINK Usage Example 3
      4. 5.4.4 AUTO_NEGOTIATE_SINK Usage Example 4
  8. 6Revision History

'DBfg' - Clear Dead Battery Flag

Table 4-16 'DBfg' - Clear Dead Battery Flag
Description The 'DBfg' Task is used to clear the dead battery flag. This Task does not disable the PP_EXT input switch that can have been enabled during dead battery operation.
INPUT DATAX None
OUTPUT DATAX None
Task Completion The 'DBfg' Task completes after the effects of clearing the Dead Battery Flag are complete.
Side Effects The Dead Battery Flag causes the PD Controller to take specific actions, so clearing this flag will have side effects. PD Controller 's power input is forced to VBUS until the Dead Battery Flag is cleared, so executing this Task will change PD Controller 's power input.
Additional Information None

There are several limitations placed on the PD controller while the Dead-Battery Flag is asserted (PowerPathStatus.PowerSource = 10b).

  • A Hard Reset will not be transmitted while in the sink role (on either port).
  • VBUS is selected as the main supply for the PD controller, even if the 3.3 V input is present.
  • The PD controller will reject PR_Swap requests to become source (on either port).
  • A port connected to a source will only act as a Type-C sink regardless of the configuration.
  • If no Source Capabilities message is received after the boot process is complete (Status.ActingAsLegacy=11b), the PD controller will not send a Hard Reset until the Dead-Battery Flag is cleared even if the SinkWaitCapTimer expires.