SLVUCR9D August   2023  – October 2026

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Revision Differences
    2. 1.2 Introduction
    3. 1.3 Kit Contents
    4. 1.4 Specification
    5. 1.5 Device Information
  8. 2Hardware
    1. 2.1 Assembly Instructions
    2. 2.2 Jumper Information
    3. 2.3 Interfaces
    4. 2.4 Test Points
    5. 2.5 Transient Testing
  9. 3Software
    1. 3.1 Software Usage
      1. 3.1.1  Command Center View
      2. 3.1.2  I2T Tuner
      3. 3.1.3  Device Settings
      4. 3.1.4  Channel Settings
      5. 3.1.5  Console View
      6. 3.1.6  Log View
      7. 3.1.7  Importing/Exporting
      8. 3.1.8  Firmware Updates
      9. 3.1.9  Persist Settings
      10. 3.1.10 Language Settings
    2. 3.2 Software Development
  10. 4Hardware Design Files
    1. 4.1 Schematics
    2. 4.2 PCB Layouts
    3. 4.3 Bill of Materials (BOM)
  11. 5Additional Information
    1. 5.1 Trademarks
  12. 6Related Documentation
  13. 7Revision History

Assembly Instructions

To get started with the HSS-HCMOTHERBRDEVM the following resources are required:

  • 1 × HSS-HCMOTHERBRDEVM
    • Firmware is pre-flashed for the EVM and no need for the user to program the EVM initially.
    • Standard USB cable included.
  • 1 × HSS-2HCS08EVM daughtercard (or any compatible Smart eFuse High-Side Switch daughtercard EVM).
  • Windows host with .NET framework run-time v4.7.2 (included in all Windows 10 versions and later).
  • Texas Instruments Smart eFuse High-Side Switch Configurator software tool (4MB).

No special drivers or large proprietary frameworks are needed to run the Smart eFuse High-Side Switch Configurator.

To get started, plug the daughtercard into the headers marked J1 and J2 on the HSS-HCMOTHERBRDEVM as seen in Figure 2-1. Note that the dots on the motherboard and daughtercard signify the pin 1 connection for proper alignment.

HSS-2HCS10EVM HSS-HCS-BLANK18EVM HSS-HCS-BLANKRBLEVM HSS-HCMOTHERBRDEVM HSS-2HCS08EVM HSS-HCS-BLANKEVM Board Alignment Figure 2-1 Board Alignment

Next, plug the USB-C cable into the HSS-HCMOTHERBRDEVM as seen in Figure 2-2.

HSS-2HCS10EVM HSS-HCS-BLANK18EVM HSS-HCS-BLANKRBLEVM HSS-HCMOTHERBRDEVM HSS-2HCS08EVM HSS-HCS-BLANKEVM USB Connection Figure 2-2 USB Connection

If successful, then the green LED on D6 illuminates and Windows automatically detects/installs the Smart eFuse High-Side Switch EVM.

Next, connect the relevant power supply to the VBB banana jack (T6) and connect the ground connection of the power supply to the GND banana jack of the EVM (T1) as seen below. Do the same for the desired load connections VOUT1 (T2) and VOUT2 (T3). Make sure that the ground connections of the loads connect back to a ground port of the EVM (such as T4).

HSS-2HCS10EVM HSS-HCS-BLANK18EVM HSS-HCS-BLANKRBLEVM HSS-HCMOTHERBRDEVM HSS-2HCS08EVM HSS-HCS-BLANKEVM Loads Connected Figure 2-3 Loads Connected

With all of the supply, loads, and USB connected, turn on the power supply to the EVM. Note that the Smart eFuse High-Side Switches used in this EVM are designed for 12V/48V automotive systems, however refer to the device datasheet for exact details on the input/output conditions supported.

With the device powered, open the auto_hss_configurator.exe executable that ships with the Smart eFuse High-Side Switch Configurator software package. Note that the software package from TI.com is a portable zip file and does not need any specific installer to operate. Once opened, the software program automatically detects the attached high-side switch and updates the connection status to Connected as seen in Figure 2-4.

HSS-2HCS10EVM HSS-HCS-BLANK18EVM HSS-HCS-BLANKRBLEVM HSS-HCMOTHERBRDEVM HSS-2HCS08EVM HSS-HCS-BLANKEVM USB Interface Detected Figure 2-4 USB Interface Detected

If the EVM is not connected, then the Connection Status shows up as Disconnected. In this state, the main elements of the GUI are disabled until the device is connected.

Note that even though the USB connection to the EVM is detected, the software interface does not enable until an active daughtercard is detected on the board. A background thread on the GUI automatically polls and checks for a valid daughtercard through a read to device register 0x00 (device ID register). If a valid ID is read, the GUI automatically enables and populates the relevant device information, shown in Figure 2-5.

HSS-2HCS10EVM HSS-HCS-BLANK18EVM HSS-HCS-BLANKRBLEVM HSS-HCMOTHERBRDEVM HSS-2HCS08EVM HSS-HCS-BLANKEVM Device Detected Figure 2-5 Device Detected

On the main interface, the status bar displays the latest command/status event that happened on the GUI. In this case, the status bar message shows that the Smart eFuse High-Side Switch device connects from the High-side switch device found and connected message. Whenever a setting is changed on the device or a significant setting is change on the GUI a message is displayed in the status bar. A timestamped list of all previous events can be seen in the Log tab as seen in Figure 2-6.

HSS-2HCS10EVM HSS-HCS-BLANK18EVM HSS-HCS-BLANKRBLEVM HSS-HCMOTHERBRDEVM HSS-2HCS08EVM HSS-HCS-BLANKEVM Log View Figure 2-6 Log View

Once connected, the GUI communicates with the EVM and read out both the device ID string as well as the firmware revision from the EVM. This information is displayed under the Detected Device section in the Command Center tab.

HSS-2HCS10EVM HSS-HCS-BLANK18EVM HSS-HCS-BLANKRBLEVM HSS-HCMOTHERBRDEVM HSS-2HCS08EVM HSS-HCS-BLANKEVM Device Information Figure 2-7 Device Information

The detailed usage guide for each of the tabs in the software can be found in the following sections.