SLVUCR9D August   2023  – October 2026

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Revision Differences
    2. 1.2 Introduction
    3. 1.3 Kit Contents
    4. 1.4 Specification
    5. 1.5 Device Information
  8. 2Hardware
    1. 2.1 Assembly Instructions
    2. 2.2 Jumper Information
    3. 2.3 Interfaces
    4. 2.4 Test Points
    5. 2.5 Transient Testing
  9. 3Software
    1. 3.1 Software Usage
      1. 3.1.1  Command Center View
      2. 3.1.2  I2T Tuner
      3. 3.1.3  Device Settings
      4. 3.1.4  Channel Settings
      5. 3.1.5  Console View
      6. 3.1.6  Log View
      7. 3.1.7  Importing/Exporting
      8. 3.1.8  Firmware Updates
      9. 3.1.9  Persist Settings
      10. 3.1.10 Language Settings
    2. 3.2 Software Development
  10. 4Hardware Design Files
    1. 4.1 Schematics
    2. 4.2 PCB Layouts
    3. 4.3 Bill of Materials (BOM)
  11. 5Additional Information
    1. 5.1 Trademarks
  12. 6Related Documentation
  13. 7Revision History

Device Settings

The Device Settings tab allows the user to change device level settings that are not specific to one channel of the device. Additionally in the Device Settings tab, all fault diagnostics are shown as well as statistics and descriptions of each individual faults (both device-wise and channel-wise). A non-faulted example of this view can be seen below.

HSS-2HCS10EVM HSS-HCS-BLANK18EVM HSS-HCS-BLANKRBLEVM HSS-HCMOTHERBRDEVM HSS-2HCS08EVM HSS-HCS-BLANKEVM Device View Figure 3-11 Device View

From here, the user can select and change any setting in the General box and the corresponding device setting is changed. Additionally, this tab shows the fault diagnostics of the device in real time. If the Setting box is set to Automatic, then a thread runs in the background that periodically polls the fault status of the device. When faulted, the corresponding fault circle changes red. The user can select any of the circles to populate the Statistics box with a description of the fault and when the last fault occurred and the total number of times that the specific fault triggered.

HSS-2HCS10EVM HSS-HCS-BLANK18EVM HSS-HCS-BLANKRBLEVM HSS-HCMOTHERBRDEVM HSS-2HCS08EVM HSS-HCS-BLANKEVM Faulted Device View Figure 3-12 Faulted Device View

In the example above, an open-load fault on channel one is reported. Note that when certain faults occur, the FAULT pin is also reported to be triggered. This pin is the open-drain fault pin that goes from the Smart eFuse High-Side Switch to the MCU.

Note that some of the device faults (such as POR) are cleared on read. This makes the device faults not desirable for the GUI to auto-poll the fault status as an important fault event can potentially be missed. To remedy this, the device can be set into Manual update mode. In this mode, the user must select the Manual Update button to read the fault status and update the indications on the GUI.