SLVUD97A September   2026  – October 2026

 

  1.   1
  2.   Description
  3.   Features
  4.   4
  5. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  6. 2Hardware
    1. 2.1 ADS9308V8IEVM Quick Start Guide
    2. 2.2 Analog Interface
      1. 2.2.1 ADC Input SMA Connections
      2. 2.2.2 Voltage Reference
    3. 2.3 Digital Interface and Clock Inputs
      1. 2.3.1 Digital Interface Connections
      2. 2.3.2 Level Translators
    4. 2.4 Power Supplies
      1. 2.4.1 USB Power and When to Power the Board Externally
  7. 3Software
    1. 3.1 ADS9308V8IEVM Software Installation
      1. 3.1.1 USB Driver Installation
    2. 3.2 ADS9308V8IEVM Software (ADS9308V8IEVM-GUI)
      1. 3.2.1 Using Configuration Tab
      2. 3.2.2 Using the Data Capture Tab
  8. 4Hardware Design Files
    1. 4.1 Schematics
    2. 4.2 PCB Layout
    3. 4.3 Bill of Materials (BOM)
  9. 5Additional Information
    1. 5.1 Trademarks
  10. 6Related Documentation
  11. 7Revision History

ADS9308V8IEVM Software Installation

This section details the installation and operation of the ADS9308V8IEVM software graphical user interface (GUI). This software requires the TSWDC155EVM (sold separately) controller to operate. The first step to installing the software (as shown in Figure 3-1) is to download the latest version of the EVM GUI installer as per Table 3-1.

Table 3-1 EVM GUI Installers
EVMSoftware Download Link
ADS9308V8IEVM

ADS9308V8IEVM-GUI

Accept all the license agreements and choose the destination location, project directory, and start menu. Typically, the default values work, but these values can be customized as needed based on the user's requirements.

Note: The GUI installer and GUI buttons can differ slightly depending on which specific GUI is being installed.
ADS9308V8IEVM Initial Software InstallationFigure 3-1 Initial Software Installation

Next, the installer prompts the user to create a desktop icon and summarize the installation plan. Selecting Install begins copying software onto the computer. This process takes a few minutes. At completion, the user can launch a readme text file and the application. Figure 3-2 shows these steps.

ADS9308V8IEVM Installation ProcessFigure 3-2 Installation Process