Download and install the ADC3669 GUI. This will be used to program the ADC.
Download and install HSDC Pro. This will be used to view the captured data.
Download and install Vivado Lab Solutions. This is required to capture data from the FPGA.
Make sure that the Vivado Lab bin folder is added to your PATH system environment variable.
Search for System
Environment Variables in the start menu
Click on Environment
Variables…
Under System Variables,
locate and click on the Path variable
Click on
Edit…
Click on New to
add a new path
Add the path to your
Vivado Lab installation, depending on where you installed Vivado Lab and
what version you installed. The path to the bin folder typically looks
something like this: C:\Xilinx\Vivado_Lab\2023.1.1\bin.