SLVUDV6A August 2026 – September 2026
This EVM revision does not follow best current sensing practice resulting in 10% to 20% current accuracy for VSNS > 10mV. This data does not match the expected performance of the TPS12S24F-Q1 part, which has been verified to match the accuracy performance specified in the datasheet.
To maximize current sense accuracy CS+/- traces must be as short as possible and length matched. In addition, avoiding vias and traces through multiple layers can further improve sensing. The next EVM revision will implement these to better demonstrate the TPS12S24F-Q1 performance. The below data represents the existing EVM performance.
To verify current sense accuracy, connect a load to the output of the tested channel.
Power on VIN = 12V
Enable CHx
Set Gain and RSNS value
Turn on load and incrementally increase current
Measure voltage across the shunt resistor with accurate DMM for each load and read back ADC ISNS value from the Device Settings tab.
Use measured VSNS value to compute actual current and compare to device ISNS
The below data captures the ISNS accuracy for both Ch1 and Ch2. The Ch1 data is significantly worse than Ch2 and will be improved in the next EVM revision with improved layout.
Figure 3-1 EVM ISNS Accuracy