The current EVM has completed all
optimization steps at this point. The Golden Gauge can program all other gauges in
production using a Golden Image and means that all gauges start with an accurate starting
point to begin reporting on and further learning about battery chemistry.
To get the necessary file for programming
gauges, follow these steps:
- Navigate to the Programming window in bqStudio.
- Choose the output directory and file name for the Golden Image under the "Path for
combined .bq.fs:" row, this becomes the .bq.fs file that contains the encrypted firmware
and the custom configuration in data flash.
- Choose the input directory and .bq.fs file for the encrypted firmware downloaded from
ti.com under the "Path for encrypted .bq.fs:" row.
- Select "Read FS from DM" to create the combined .bq.fs Golden Image file that can be
programmed onto other battery packs in production