SLVUDY5A July 2026 – July 2026
This section describes the test points and connectors on the EVM and how to properly connect, set up, and use the LMR61440QEVM.
The EVM uses the LMR61440-Q1 converter, which includes MODE/SYNC capability. This capabilityu means that the device can operate in pulse frequency modulation (PFM) light-load mode when this pin is tied to GND. TI has observed additional output voltage ripple at input voltages close to the output voltage when the device is operating in PFM light-load mode. To see improved performance, TI recommends to configure the EVM to operate in forced pulse width modulation (FPWM) mode.
The test setup consists of the following instruments in addition to the EVM board:
A load transient generator is provided on the EVM. Connect a suitable pulse generator to the "LS_gate" SMB connector and adjust the load current pulse amplitude and duration as desired, while monitoring the voltage at J2. A 10mΩ sense resistor is used, providing a scale factor of 10mV/A. The pulse duty cycle must be kept low to avoid damaging the MOSFET. The output voltage can be monitored use the VOUTS SMB or directly across the output capacitors. TI recommends use of a high speed differential probe. See also Figure 2-2.