The TMAG5230 operates as a duty-cycled
device, periodically measuring the magnetic flux density, updating the output, and entering a
low-power sleep state between measurements to conserve power.
Figure 7-7 displays the start-up behavior of the TMAG5230 and some examples of the active low
omnipolar output pin voltage based on different magnetic flux density value scenarios. When
the minimum value for V
CC is reached, the TMAG5230 takes time t
ON to
power up, measure the first magnetic sample, and set the output value. When the output value
is set, the output is latched and the device enters a low power sleep state. After each
t
S time has passed, the device measures a new sample and updates the output if
necessary. If the magnetic field does not change between periods, the output also does not
change.