SLYT818 November   2021 LM74701-Q1 , LM74721-Q1

 

  1. 1 Introduction
  2. 2 Automotive reverse-battery protection with ideal diode controllers
  3. 3 TVS-less automotive reverse-polarity protection using ideal diode controllers
  4. 4 TVS-less ideal diode: mode of operation and working principle
  5. 5 External MOSFET
  6. 6 Output Capacitor (COUT)
  7. 7 TVS-less ideal diode controller EMC performance
  8. 8 Conclusion
  9. 9 Related Websites
  10. 10Important Notice

External MOSFET

Select an external MOSFET that achieves the best trade-off between power dissipation, system-level performance (such as reverse-current blocking) and solution cost. A MOSFET that typically provides 30 mV to 50 mV of forward drop at a full load current is a good starting point.

Another important parameter is the MOSFET’s maximum VDS voltage rating. During the ISO 7637-2 Pulse 1 transient event, the maximum VDS seen by the external MOSFET Q1 is the VDSCLAMP (max) detection threshold of an ideal diode controller. Equation 1 calculates the peak current flowing through the MOSFET during the ISO 7637-2 Pulse 1 transient event:

Equation 1. I I S O _ P E A K =   ( V I S O +   V O U T -   V D S C L A M P max ⁡ ) R S

where:

VISO is the negative peak of ISO 7637-2 Pulse 1 transient event,

VOUT is the initial level of the VBATT before applying the ISO 7637-2 Pulse 1,

VDSCLAMP is the maximum VCLAMP threshold of the ideal diode controller and

RS is the ISO 7637-2 pulse-generator input impedance (10 Ω).

Figure 5-1 shows the LM74701-Q1’s TVS-less performance during ISO 7637-2 Pulse 1 transient event, along with gate turn on behavior during VDS clamp operation, peak pulse current and power dissipation across the MOSFET.

GUID-20211026-SS0I-JMWB-XLPK-H9TJRK678PXF-low.png Figure 5-1 LM74701-Q1 ideal diode controller TVS-less performance.

The average current during an ISO 7637-2 pulse can be approximated as one-third the peak current, or (IISO_PEAK/3). So Equation 2 calculates the average power dissipated across the external MOSFET:

Equation 2. P D _ I S O _ A V G =   V D S C L A M P   ( max ⁡ )   ×   I I S O _ P E A K 3  

An ISO 7637-2 Pulse 1 transient event lasts for typically 2 ms, and the external MOSFET operates in active clamp mode for about 1 ms. Selecting a MOSFET with safe operating area (SoA) characteristics – with the load line corresponding to the VDS of VDSCLAMP (max) and drain current (ID) greater than (IISO_PEAK/2) for 1 ms is a suitable option.

Figure 5-2 shows typical SoA characteristics and example selection criteria for the MOSFET.

GUID-20211026-SS0I-DKFR-FZ85-B37TKMGCP5VV-low.png Figure 5-2 Example MOSFET SoA selection curve.