SLYT877 April 2026 LMG3427R030 , TMS320F280039C
For TCM control, adding a zero current detection (ZCD) circuit by placing a resistor on the PFC ground return path or adding a second winding on the boost inductor will detect the instant that the inductor current drops to zero. Some devices, such as TI's LMG3427R030 gallium nitride (GaN) field-effect transistor (FET), have a built-in ZCD circuit, generating a ZCD signal when the current goes to zero, as shown in Figure 3. Using this device as a high-frequency switch can significantly simplify the design process. The ZCD signal is sent to a microcontroller (MCU) for further processing.