SNAA434 March 2025 LMX2820
Start by thinking about adding two vectors of equal magnitude. The first vector is at angle of zero degrees and the second is at angle of ϕ. The vector is therefore:
<1+cos ϕ, sin ϕ>The magnitude can be calculated to be:
If not intuitive that the angle of the resultant vector is, then this becomes more apparent by recognizing the angle as calculated by this vector relates to the half angle formula for tangent.
Furthermore, this needs to be intuitive that if one combines an even number of vectors, the angle does not change and the magnitude can be:
If there is an odd number of vectors, then add all but the last one and this formula is known. Clearly if the last vector was at angle f/2, then this can give the most power, so without loss of generality, this can be at zero degrees for the worst case. So in the case of an odd number of vectors, the magnitude can be:
Of interest is the loss in power compared to the designed for combination of N signals and this can be calculated as: