SNAS693D July 2017 – February 2021 HDC2010
PRODUCTION DATA
The only component next to the device is the supply bypass capacitor. The relative humidity is dependent on the temperature, so the HDC2010 should be positioned away from hot spots present on the board, such as a battery, display or microcontroller. Slots around the device can be used to reduce the thermal mass for a quicker response to environmental changes.
Figure 10-1 HDC2010 PCB Layout Example