SNAS871B July 2025 – August 2026 LMR60406-Q1
PRODUCTION DATA
| PIN | TYPE(1) | DESCRIPTION | |
|---|---|---|---|
| NO. | NAME | ||
| 1 | VIN | P | Regulator input power pin to
the high-side power MOSFET and internal VCC regulator. Connect to the input supply and the positive terminal of the input filter capacitor. The path from the VIN pin to the input capacitor must be as short as possible. |
| 2 | PGND | G | Power ground. This pin connects to the source of the low-side MOSFET internally. Connect to system ground, and the ground terminal of the CIN and COUT capacitors. The path to CIN must be as short as possible. |
| 3 | SW | P | Regulator switch node. Connect to the power inductor and bootstrap capacitor. |
| 4 | BOOT | P | High-side MOSFET driver
supply for bootstrap gate drive. Connect a high quality 100nF capacitor between this pin and SW as close to the device as possible. |
| 5 | PG | O | Open drain power-good
output. Connect to a suitable voltage supply through a current limiting pullup resistor. High = regulator power good, Low = output out of regulation. Goes low when EN = low. See also Section 7.3.8. |
| 6 | FB | I | Feedback pin. Connect this pin directly to the output voltage node for fixed VOUT operation. See Section 4 for the voltage level for each device variant. Connect to the center point of a feedback voltage divider placed between VOUT node and PGND to program an adjustable output voltage. |
| 7 | MODE/SYNC | I | Operational mode input
pin. Connect this pin to the RT pin to select FPWM switching or connect this pin to PGND to select PFM switching at light loads. To synchronize to an external clock, connect a 100kΩ resistor to ground and drive directly from the clock. See the Electrical Characteristics table for acceptable voltage levels and timing requirements. |
| 8 | RT | I | Frequency programming
pin. A resistor from RT to PGND sets the oscillator frequency between 200kHz and 2.2MHz. |
| 9 | EN | I | Enable pin for the
regulator. Drive this pin high to enable the device and low to disable the device. If the enable function is not needed, connect this pin to the VIN pin. See the Electrical Characteristics for more information on acceptable voltage levels. |