The LMR60440-Q1 is in
an active mode whenever the EN pin voltage has risen above VEN-TH(R), the
input voltage exceeds VINUVLO(R), and no other fault conditions are
present. The simplest way to enable the LMR60440-Q1 is
to connect the EN pin to VIN, which allows self start-up when the applied input
voltage exceeds the VINUVLO(R).
In active mode, the LMR60440-Q1 is in one of the
following modes:
- Continuous conduction mode (CCM) with fixed switching frequency when the
load current is above half of the inductor current ripple
- Auto mode - light load
operation: pulse frequency modulation (PFM) where switching frequency is
reduced at light load
- FPWM mode - light load operation: CCM mode when the load current is lower
than half of the inductor current ripple
- Minimum on-time: at high
input voltage and low output voltages, the switching frequency is reduced to
maintain regulation
- Dropout mode: when switching
frequency is reduced to minimize voltage dropout between input and
output