SNAS875A February 2025 – June 2025 LMR60430-Q1
PRODMIX
The LMR60430-Q1 device can be configured to operate in either fixed or adjustable output voltage modes. For fixed output voltages as specified by the device orderable part number, simply connect the output voltage rail directly to the FB pin. When other output voltages are required, a resistor divider between the output voltage rail and ground with the FB pin as the center point set the output. Use the folloing equation to calculate the output voltage given a specific feedback divider.
Alternatively, if the output voltage and RFBT are already known, use the following equation to calculate the value of RFBB.
Note that typically 100kΩ is used for RFBT.