SNAU298 October 2023
Figure 5-1 show the typical phase noise performance for 156.25 MHz reference clock input using a SMA100B.
LMKDB1120EVM was configured in cascaded mode to get these measurements:
As shown below in Figure 5-1, reference input jitter is 36.7 fs. As shown in Figure 5-2, measured jitter on the output of LMKDB1120 is 43.7 fs. Calculated typical additive jitter is about 24 fs for the LMKDB1120.