SNLA343A April 2020 – July 2021 DP83825I
Figure 2-1, is a Sitara MDIO / MII arch example. In the Figure 2-1, the MDIO is a control interface to control the Phy (example: DP83825), and the MII is an interface for the Data Channel between CPU and Phy.
Figure 2-1 Sitara MDIO / MII Arch
ExampleFigure 2-2, show an example that the MII can be replaced by the other Ethernet Phy spec, for example (RMII, RGMII, SGMII and so on). MDIO control interface can be replaced by I2C/SPI.
While using TI Sitara platform to adapt the TI Phy, we are continuing with MDIO. The EMAC in the Figure 2-2 is an Ethernet MAC layer.
Figure 2-2 Sitara MDIO / MII Detail
Arch