SNLA433B August 2023 – January 2026 DS320PR1601 , DS320PR410 , DS320PR810 , SN75LVPE5412 , SN75LVPE5421
PCI-Express (PCIe) links are typically implemented with 4-lane (x4), 8-lane (x8), and 16-lane (x16) widths. Bidirectional communication between a PCIe root complex (RC) and a PCIe endpoint (EP) is carried over downstream (from RC to EP) and upstream (from EP to RC) channels.
Figure 2-3 Diagram of a PCIe LinkTransmission media between a PCIe transmitter (TX) and a redriver is a pre-channel, while a channel between a redriver and a PCIe receiver (RX) is a post-channel, indicating the channels' positions relative to the redriver. It is important to note that the pre-channel loss compensation is handled by both PCIe TX equalization and the redriver CTLE.
For systems approaching or surpassing the total system loss budget of 36dB, it is recommended to use higher-grade, low-loss materials such as Megtron-6 and also recommended to place the redriver such that the loss between CPU and redriver is approximately 27-36dB, allowing the redriver to compensate for the additional system loss.
To check RX EQ compliance, the Phoenix utility is used to do post processing to check that the eye margin conforms to PCIe Gen5 requirements. This post processing involves PCIe Gen5 RX package compensation, behavioral CTLE/DFE, and CDR implementation. This calls for 15 mv vertical eye opening with at least 0.3 UI or 9.375 ps horizontal eye opening. A series of tests—using a BERT with the P9 preset and 800 mVpp amplitude—are done to show redriver ISI or DJ compensation capabilities. In these tests, different pre- and post-channel losses are used.
As shown in Figure 2-3, for pre- and post-channel losses of 20 dB, a Gen5 redriver with a CTLE setting of 0 can meet PCI-SIG requirements.
Figure 2-4 PCIe Link Analysis Example with 20 dB Pre-channel, 20-25 dB Post-channelIn Figure 2-5 and Figure 2-6, we are using a higher pre-channel loss (30 dB) with the same earlier variations of post-channel loss. The redriver mainly compensates for the pre-channel loss and can perform marginal over-compensation to address the increase in pre-channel loss.
Figure 2-5 PCIe Link Analysis Example with 30 dB Pre-channel, 20-25 dB Post-channel
Figure 2-6 PCIe Link Analysis Example with 35 dB Pre-channel, 20-25 dB Post-channelAs shown, the redriver compensates for the ISI (Inter-Symbol-Interference) on the input due to the transmission media low-pass filtering effects. Either the RC or the EP can compensate for the stressed eye diagram due to other factors: random jitter (RJ), sinusoidal jitter (SJ), reflections caused by impedance discontinuities, skew from mismatched trace lengths, and differential and common mode interferences.