SNLU296A December 2022 – December 2022
The Device Status tab shows a high level overview of the status of each channel in the DS560MB410. Although a summary of channel settings can be viewed from this this tab, they cannot be changed from this tab. Channel settings that are displayed in this tab can be changed from the Block Diagram tab.
Figure 5-7 Device Status Tab|
Seting or Button Name |
Behavior |
|---|---|
| Update Time | Sets the time interval at which the device status is updated. This is only in use while Continuous Status Update is checked. |
| Channel Select | This setting is persistent when switching between the Device Status, Block Diagram, and Crosspoint Switch tabs. This selection is only used in the Block Diagram tab. |
| Refresh From Device | Reads register data from the device. This data will then be updated in the DS560MB410 Profile pages. |
| Reset Device | Resets all device registers to their default values. |
| Load From File | Opens a window allowing the user to select a file with register data. Once the appropriate file is selected, register data from the file will be written to device registers. |
| Save To File | Opens a window enabling the user to save device register data to their computer. This file contains data for all of the device registers. |
| Continuous Status Update | When checked, the registers from the device will be polled at the rate set by the Update Time setting. |