SNOAA62B February 2023 – October 2024 LMP7704-SP
The primary single-event effect (SEE) events of interest in the LMP7704-SP are single-event latch-up (SEL). From a risk and impact point-of-view, the occurrence of an SEL is potentially the most destructive SEE event and the biggest concern for space applications. The VIP050 process was used for the LMP7704-SP. CMOS circuitry introduces a potential for SEL susceptibility. SEL can occur if excess current injection caused by the passage of an energetic ion is high enough to trigger the formation of a parasitic cross-coupled PNP and NPN bipolar structure (formed between the p-sub and n-well and n+ and p+ contacts). The parasitic bipolar structure initiated by a single-event creates a high-conductance path (inducing a steady-state current that is typically orders-of-magnitude higher than the normal operating current) between power and ground that persists (is latched) until power is removed or until the device is destroyed by the high-current state.
The initial characterization study was performed to evaluate the SEL effects with a bias voltage of 5.5V on VIN and supply voltage of 12V (VS = ±6V). Heavy ions with LETEFF = 85MeV-cm2/mg were used to irradiate the devices. Flux of 105 ions/s-cm2 and fluence of 107 ions/cm2 were used during the exposure at 125°C. The VIP050 process modifications applied for SEL mitigation were shown to be sufficient because the LMP7704-SP exhibited no SEL with heavy-ions up to an LETEFF of 85MeV-cm2/mg at a fluence of 107 ions/cm2 and a chip temperature of 125°C.

Subsequent analysis and retesting of the device identified a vulnerability in the device architecture, with one subcircuit having the potential to cause device burnout under specific circuit criteria. Though the activation of this vulnerability does not give rise to a parasitic bipolar structure, an unintended high-conductance path between V+ and V– still results. If enough current flows along this path, the resulting electrical overstress and associated localized heating can destroy the device. Because the structure can only be activated by a high-energy particle, the scenario is classified as a SEL. See Section 7 for detailed discussion of this vulnerability, including root cause.