SNOAA84A January 2022 – February 2022 LM4050QML-SP , LMP7704-SP
Design Simulations
The following plots show the output voltage across the 2.49-kΩ (R3) resistor. The error is calculated based on the following equation:

Ideally, Vout swings from 0 V to 5 V as the load current (Iload) swings from 0 A to 10 A. However, the minimum of Vout is 373 mV and is non-linear before the load current (Iload) gets up to 735 mV.

The following simulation and calculations show the power consumption of each component in the circuit with different load currents. Without considering the power consumption on the R_shunt, the overall power rate is from 471.4 mW to 651.3 mW. R2 dominates the power consumption.


The following figure shows the gain of the circuit, where Gain = Vout (V) / Iload (A). With a load capacitance of 15 pF, the 1% full power bandwidth and the 3-dB bandwidth is found to be 478 kHz and 3.8 MHz.

The stability of the system is verified by measuring its phase margin and applying a small signal-transient step response. To ensure stability, the phase margin, which is measured at a point where the Aol curve intersects 1/β, needs to be at least 45 degrees.
As shown in the following schematic, a 1-μF capacitor is added in the feedback loop to increase stability. The following open-loop AC simulation breaks the loop at the input and the following equations are used to plot the relevant curves:


The previous image shows the frequency domain simulation result. The phase margin is measured at a point where 1/ꞵ and Aol intercept, and it is 58.3 degrees, indicating the system is stable.
To further ensure stability, a small signal transient step response is applied at the input (IG1) of the circuit and percent overshoot is measured at Vo. The overshoot in the following image indicates a phase margin of 59 degrees, further confirming the stability of the system.


It is necessary to put a 10-kΩ pullup resistor (R1) in front of the PMOS gate to pull up the PMOS gate and protect the ADC or microcontroller.
Another fault consideration is whether the op amp (LMP7704-sp) will get damaged by the 100-V Vbus. To simulate it, a 100-V peak-to-peak square wave is applied to the Vbus. See the simulation results in the following image.

V_opamp, which is the difference between Vbus and VEE, is always below 4.933 V. LMP7704 is designed for a power supply up to 12 V, so it will not be damaged. Load current is set to 5 A in the simulation. As expected, Vout is simulated to be around 2.5 V.
To analysis the output error of the circuit, the following parameters are needed
Offset error:

CMRR error:

PSRR error:

Shunt resistor error:

Resistor (R3 and R6) error:

Bias current error:

Root Sum Square (RSS) total error:

Extreme Value Analysis (EVA):

The previous error equations are implemented in MATLAB, and the simulation result is shown in the following image.

The RSS is 0.658% when the load current is 1 A. This RSS satisfies the 0.7% error requirement. The EVA plot is also provided on the right as a reference.

The previous result is calculated with R_shunt set to 10 mΩ. When the load current is 1 A, the op amp Vos dominates the error. When load current is 10 A, the shunt resistor tolerance dominates the error.
The previous error calculation is verified again with TINA-TITM simulation, and the result is shown in the following image.

The percent error is calculated with the following equation.

As shown in the simulation, when the load current is 1 A, the error is 0.63%. This error is consistent with the 0.6% Vos error in the previous MATLAB calculation. TINA-TITM does not simulate the error caused by resistor tolerance and changing temperature on the shunt resistor.