SNOSD17G October 2017 – December 2020 LM74700-Q1
PRODMIX
Figure 5-1 DBV Package6-Pin SOT-23Top View| PIN | I/O(1) | DESCRIPTION | |
|---|---|---|---|
| NO. | NAME | ||
| 1 | VCAP | O | Charge pump output. Connect to external charge pump capacitor |
| 2 | GND | G | Ground pin |
| 3 | EN | I | Enable pin. Can be connected to ANODE for always ON operation |
| 4 | CATHODE | I | Cathode of the diode. Connect to the drain of the external N-channel MOSFET |
| 5 | GATE | O | Gate drive output. Connect to gate of the external N-channel MOSFET |
| 6 | ANODE | I | Anode of the diode and input power. Connect to the source of the external N-channel MOSFET |
Figure 5-2 DDF Package8-Pin SOT-23Top View| PIN | I/O(1) | DESCRIPTION | |
|---|---|---|---|
| NO. | NAME | ||
| 1 | EN | I | Enable pin. Can be connected to ANODE for always ON operation |
| 2 | GND | G | Ground pin |
| 3 | N.C | No connection | |
| 4 | VCAP | O | Charge pump output. Connect to external charge pump capacitor |
| 5 | ANODE | I | Anode of the diode and input power. Connect to the source of the external N-channel MOSFET |
| 6 | GATE | O | Gate drive output. Connect to gate of the external N-channel MOSFET |
| 7 | N.C | No connection | |
| 8 | CATHODE | I | Cathode of the diode. Connect to the drain of the external N-channel MOSFET |