SNOU181B February 2021 – April 2022 LDC3114 , LDC3114-Q1
The Registers page allows the user to read and write to the device registers. Additionally, the Auto Read function will default to Off, but can be set to the following speeds:
The data registers have been combined onto a single line in the GUI for ease of use, but they are still separate 8-bit registers in the device. The firmware on the EVM reads the needed registers for a given channel and combines them in the proper order before reporting the data to the GUI.
Figure 2-3 Registers Page.