SNOU197 july 2023
C16, C17, C18, and C19 are installed with 0.1-uF capacitors. If a 100-Ω differential probe is unavailable to measure the LVDS output, then these capacitors allow for the AC portion of the signal to be seen on a 50-Ω terminated scope. Keep in mind that any duty cycle other than 50% results in a DC portion of the signal that is not halfway between VOH and VOL. As mentioned earlier, this is due to the charging and discharging of the capacitors. A higher duty cycle results in a higher DC output voltage because the capacitors are charging more than the capacitors are discharging.