The inductor is selected according to three main
parameters: calculated inductance value (LM), RMS inductor current and
the maximum peak inductor current (ILPEAKlimit).
- The inductance is selected to be 2.6 µH. This value is a standard inductance
value supplied by many magnetic vendors.
- The inductor RMS current is approximated by the average supply current at the
minimum supply voltage, maximum load target voltage and maximum output power, 25
A. The inductor RMS current rating should be higher than the estimated RMS
current and keep the inductor temperature to suitable level based on the
application.
- The saturation current of the inductor should be larger than
the maximum peak inductor current limit, 40A. The magnetic material and
constructions of the inductor dictate the saturation profile. A hard saturation
profile has a dramatic decrease in inductance when the inductor becomes
saturated, while a softer saturation profile has a slower roll off. Check the
inductor data sheet to ensure the saturation is above the peak inductor current
limit.
For this design example, the inductor is selected
to have an inductance value of 2.6 µH, a saturation current limit of 50 A, and a
30°C temperature rise at 25 A RMS.