SNVSCM3 June 2024 LM5171
PRODUCTION DATA
The example circuit uses UVLO pin as the Controller enable pin of LM5171. However, UVLO pin can also fulfill the function of undervoltage lockout, either the 48V rail UVLO, or 12V rail UVLO, or VCC UVLO.
Assume the user implements the 48V rail UVLO, and the low-side resistor RUVLO2 = 10kΩ, the 48V UVLO release threshold VUVLO = 24V, and UVLO hysteresis is VHYS = 2.4V. Referring to Figure 6-32 and Equation 20, one can find that RUVLO1 is given by:

The final selection must select the closest standard resistor of RUVLO1 = 86.6kΩ.
And RUVLO3 must satisfy Equation 22, namely,

Select the closest standard resistor, RUVLO1 = 976Ω.
If the user chooses to add the capacitor CUVLO = 1nF, it leads to a delay time constant of 10µs to filter possible noise at the at the UVLO pin.