SNVSCM5A January 2024 – April 2026 LMR43606-Q1
PRODUCTION DATA
Any time the output voltage falls more than a few percent, output voltage ramps up slowly. This condition, called graceful recovery from dropout in this document, differs from soft start in two important ways:
Figure 7-10 Recovery from DropoutWhether output voltage falls due to high load or low input voltage, after the condition that causes output to fall below the set point is removed, the output climbs at the same speed as during start-up. shows an example of this behavior.