SNVSCS1 November 2025 LM25190-Q1
PRODUCTION DATA
The LM25190-Q1 contains gate drivers and an associated high-side level shifter to drive the external N-channel power MOSFETs. The high-side gate driver works in conjunction with an internal bootstrap diode DBOOT and bootstrap capacitor CBOOT. During the conduction interval of the low-side MOSFET, the SW voltage is approximately 0V and CBOOT charges from VCC through the internal DBOOT. TI recommends a 0.1μF ceramic capacitor connected with short traces between the CBOOT and SW pins.
The HO and LO outputs are controlled with an adaptive dead-time methodology so that both outputs (HO and LO) are never on at the same time, preventing cross conduction. Before the LO driver output is allowed to turn on, the adaptive dead-time logic first disables HO and waits for the HO voltage to drop below 1.5V typical. LO is allowed to turn on after a small delay (HO fall to LO rising delay). Similarly, the HO turn-on is delayed until the LO voltage has dropped below 1.5V. This technique makes sure of adequate dead-time for any size N-channel power MOSFET implementations, including parallel MOSFET configurations.
Caution is advised when adding series gate resistors, as this addition can impact the effective dead-time. The selected high-side MOSFET determines the appropriate bootstrap capacitance value CBOOT in accordance with Equation 14.
where
To determine CBOOT, choose ΔVCBOOT such that the available gate drive voltage is not significantly impacted. An acceptable range of ΔVCBOOT is 100mV to 300mV. The bootstrap capacitor must be a low-ESR ceramic capacitor, typically 0.1µF. Select FETs to make sure that the minimum input supply voltage is higher than gate plateau voltage of the FET plus 0.5V so that the FET works in the ohmic region when turned on.
When the LM25190-Q1 is configured for a target output voltage smaller than 7.5V, the internal bootstrap UV circuit can source a 25uA current out of the SW pin. In the light load or no load case where the resistance of the feedback divider is not low enough to sink the extra amount of current, some dummy load is required to bleed off the charge on the output capacitors.