SNVU682A July 2019 – March 2021
This section describes the connectors and the test points on the EVM.
VIN_EMI terminal connects to the input capacitors and the VIN pins of the LM61495-Q1 through an input EMI filter. Connect the supply voltage (battery, bench-top supply, or other supply) between VIN_EMI and GND_EMI connectors. The voltage range should be higher than 3.5 V for the device to start up, and above 3V to continue operation. VIN higher than 6 V provides regulated 5 V output voltage. VIN should be no higher than 36 V to avoid damaging the device. The current limit on the supply must be high enough to provide the needed supply current, otherwise the supply voltage may not maintain the desired voltage. The supply voltage should be connected to the board with short, thick wires to handle the pulsing input current.
This is the current return path for the supply connected to VIN_EMI.
VOUT terminal connects to the power inductor and the output capacitors. Connect the loading device between VOUT and GND connectors on J2 to load the converter output. Connect the loading device to the board with short, thick wires to handle the large DC output current.
This is the current return path for the output voltage connected to VOUT.
The input filter consists of a ferrite bead, filter inductor, and filter capacitors, located on the bottom side of the PCB. The output of the filter is connected to the VIN net, which is connected to the VIN pins of the LM61495-Q1 and the input capacitors.
Conducted EMI arises from the normal operation of switching circuits. The ON and OFF actions of the power switches generate large discontinuous currents. The discontinuous currents are present at the input side of buck converters. Voltage ripple generated by discontinuous currents can be conducted to the voltage supply of the buck converter via physical contact of the conductors. Without control, excessive input voltage ripple can compromise operation of other devices connected to the source. The input filter helps to smooth out the voltage perturbations leading to the source.
Plate the shunt to connect VOUT to BIAS to improve efficiency.
Place the shunt connecting FB and 5V to set VOUT = 5V. Place the shunt connecting FB and 3.3V to set VOUT = 3.3V.