SNVU923B December 2024 – December 2025
The LMG5126 can be configured using three pins SYNCOUT, CFG1 and CFG2. In the LMG5126EVM, these pins can be configured through the five DIP switches by selecting one of the 16 levels presented for each of the two configuration pins when the jumpers on connectors JP6 and JP7 are connecting CFG1 to DIP1 and CFG2 to DIP2, respectively. Each DIP switch has eight toggling switches that either connects or disconnects a fixed valued resistor from the configuration pins. At one time, there can be only one of the 16 levels, for each configuration pin, selected to configure the LMG5126 as seen below and according to the information given on the LMG5126 Wide-Input, 2.5MHz, Boost Converter data sheet.
The SYNCOUT-pin defines the overvoltage protection level and the ATRK, DTRK-pin 20uA current used for output voltage programming by resistor.
| Level | OVP level | 20μA ATRK current |
|---|---|---|
|
1 |
25V |
ON |
|
2 |
25V |
OFF |
|
3 |
35V |
ON |
|
4 |
35V |
OFF |
|
5 |
50V |
ON |
|
6 |
50V |
OFF |
|
7 |
65V |
ON |
|
8 |
65V |
OFF |
The CFG1-pin setting defines the clock dithering, the peak current limit (ICL_latch) operation, current sense voltage level and the gate driver strength.
| Level | Spread Spectrum | Sense Voltage | ICL_latch | Gate Drive Strength |
|---|---|---|---|---|
|
1 |
DRSS ON |
30mV |
Enabled | Weak |
|
2 |
DRSS ON |
60mV | Enabled | Weak |
|
3 |
DRSS ON |
30mV | Enabled | Strong |
|
4 |
DRSS ON |
60mV | Enabled | Strong |
|
5 |
DRSS ON |
30mV | Disabled | Weak |
|
6 |
DRSS ON |
60mV | Disabled | Weak |
|
7 |
DRSS ON |
30mV | Disabled | Strong |
|
8 |
DRSS ON |
60mV | Disabled | Strong |
|
9 |
DRSS OFF |
30mV |
Enabled | Weak |
|
10 |
DRSS OFF |
60mV | Enabled | Weak |
|
11 |
DRSS OFF |
30mV | Enabled | Strong |
|
12 |
DRSS OFF |
60mV | Enabled | Strong |
|
13 |
DRSS OFF |
30mV | Disabled | Weak |
|
14 |
DRSS OFF |
60mV | Disabled | Weak |
|
15 |
DRSS OFF |
30mV | Disabled | Strong |
|
16 |
DRSS OFF |
60mV | Disabled | Strong |
The CFG2-pin defines if the device is configured for a single-or multichip setup, which then defines the operation mode of SYNCIN and SYNCOUT pin. PGOOD OVP can also be set.
| Level | Single or Multichip | SYNCOUT | SYNCIN | PGOOD OVP Enable |
|---|---|---|---|---|
|
1 |
Single |
OFF |
OFF |
ON |
|
2 |
Single |
OFF |
ON |
ON |
|
3 |
Primary |
90° |
ON |
ON |
|
4 |
Primary |
120° |
ON |
ON |
|
5 |
Primary |
180° |
ON |
ON |
|
6 |
Secondary |
OFF |
ON |
ON |
|
7 |
Secondary |
90° |
ON |
ON |
|
8 |
Secondary |
120° |
ON |
ON |
|
9 |
Single |
OFF |
OFF |
OFF |
|
10 |
Single |
OFF |
ON |
OFF |
|
11 |
Primary |
90° |
ON |
OFF |
|
12 |
Primary |
120° |
ON |
OFF |
|
13 |
Primary |
180° |
ON |
OFF |
|
14 |
Secondary |
OFF |
ON |
OFF |
|
15 |
Secondary |
90° |
ON |
OFF |
|
16 |
Secondary |
120° |
ON |
OFF |
S1 through S5 are 8-bit DIP switches.
Select position 7 for S1 by default to set level 7 for SYNCOUT:
Select position 2 for S3 by default to set level 10 for CFG1:
Select position 1 for S4 by default to set level 1 for CFG2: