SPIU024 November   2026

 

  1.   1
  2.   Description
  3.   Resources
  4.   Features
  5.   Applications
  6. 1System Description
  7. 2System Overview
    1. 2.1 Block Diagram
    2. 2.2 Design Considerations
    3. 2.3 Highlighted Products
  8. 3Hardware, Software, Testing Requirements, and Test Results
    1. 3.1 Hardware Requirements
    2. 3.2 Software
    3. 3.3 Test Setup
    4. 3.4 Test Results
      1. 3.4.1 ADS-B 1090ES Dynamic Range ve Packet Error Rate (PER)
      2. 3.4.2 ADS-B 1090ES Field Testing
  9. 4Design and Documentation Support
    1. 4.1 Design Files
      1. 4.1.1 Schematics
      2. 4.1.2 BOM
    2. 4.2 Tools and Software
      1. 4.2.1 Software
    3. 4.3 Documentation Support
    4.     Trademarks

ADS-B 1090ES Dynamic Range ve Packet Error Rate (PER)

Test Procedure:

  1. Setup the test and VSG
    1. Follow the test setup as shown in Figure 3-1.
    2. On the waveform generator, which is being used as an external trigger, turn on the output and then put it in manual trigger mode. Then, set the burst to 100 cycles of a square wave at 50Hz and a Vpp of 3V.
    3. Load the ADS-B waveform file to the ARB generator of the VSG.
    4. Verify that the ADS-B waveform parameters are as expected.
    5. Set the VSG to external trigger mode, enable the baseband, I/Q and RF modulation.
    6. Set the VSG to 1.09GHz and power level of the VSG to -30dBm.
  2. Calculate the baseline input power to the device.
    1. Before starting testing, it is important to connect the output of the signal generator directly into a network analyzer to take note of the baseline input power being fed into the device.
    2. Input power at the same power level will be dependent on environmental facts and will vary across setups. This will then be added to the total dB of the attenuator to become the total input power.
    3. In this example, the baseline power was –24dBm and the attenuator value at Pmax was 13dB which then produced the total input power of –37dBm as seen in the table below.
  3. Transmit to calculate packet error rate (PER)
    1. Set the attenuator to –60dB attenuation and start transmitting.
    2. Once transmitting, monitor the UART transmission line with a UART monitoring program that compares number of packets sent using the external trigger to the known good packet data to calculate PER
    3. After all expected packets are sent, decrease the level of attenuation and retransmit ADS-B again until PER is above desired threshold

Shown in Table 3-1 is the dynamic range calculated based on a 5% PER threshold and measured at RF port:

Table 3-1 Dynamic Range
Test Conditions Sensitivity (dBm) Saturation limit (dBm)
DSA = 0dB -86 -54
DSA = 15dB -70 -38