SPRACV2 November 2020 AWR1843 , AWR2243
In single chip usage, the self-calibrations/run time calibrations reconfigure the analog sections in 10°C temperature bins to mitigate temperature effects. If the devices in a cascade system are allowed to calibrate independently (e.g. in automatic periodic calibration mode), it is possible that they make calibration updates at different times, depending on their individual temperatures. Because each device’s analog reconfiguration can change its phase responses, these calibration updates can cause abrupt jumps in inter-channel imbalances of the cascade system (see graphs illustrating this in later sections of this note). They also cause abrupt changes in the radar return signal’s absolute phase over time and corrupt advanced single-chip algorithms.
To avoid such jumps, TI recommends that the customer use a factory calibration procedure for the sensor (described in subsequent sections) and during the live operation in the field, the host processor take control of the calibration triggers by using a certain Temperature Index Update sequence to reconfigure the AWR devices and compensates for the expected phase jump in the processing.