SPRAD98A May 2023 – November 2026 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
Industries rely on automation to increase production rates and overall efficiencies. To raise the productivity, companies are deploying robots in factories and humans continue to work alongside these machines. As a result, employees are exposed to new types of hazards that require regulation to provide personal safety. To show that robots meet safety requirements, prior to being released to the market, each product must go through a safety assessment. Assessments must show that machines meet the minimum safety requirements based on the necessary Type C product safety standard. Figure 1-1 shows some typical standards used for robotic applications and shows how these standards connect with each other. Different standards can be used for arguing a robotic implementation which is integrated for different purposes.
Demonstrating that the product is safety-compliant is typically a long and complex procedure, which increases the overall design cost, robot size, and time-to market. This white paper offers a simplified explanation of the process to follow for conducting a safety assessment of a motor drive. The assessment uses the Type C standard of the ISO 3691-4 standard. The Type C standard defines the type of safety architecture and performance level that is required for the assessment. In this use-case, the ISO 3691-4 standard refers to the ISO 13849 standard and the safety performance level d (PLd). The implementer must determine whether to design a category 3 (CAT3) PLd system or a category 2 (CAT2) PLd system. In this use-case, cost and size are critical; therefore, an analysis was included for a block-level concept of how to achieve CAT2 using a safety rated component by TI. In this use-case, the block-level system was shown to achieve a PLd of CAT2, according to the ISO 13849 standard, or a safety integrity level 2 (SIL 2) and hardware fault tolerance (HFT) equal to zero, according to the IEC 60204-1 standard. This use-case is intended to help readers effectively meet the safety requirements of ISO 3691-4 while maintaining a smaller BOM size, potentially at a lower cost. The ISO 3691-4 (section 4) standard is the standard for industrial trucks; however, section four of the standard also covers autonomous trucks, which are used as the state-of-the art standard when developing autonomous mobile robots (AMRs) for warehouse environments. The procedure used in this use-case can be used with any other machinery that requires a PLd of Cat 2 for safety.
This concept uses TI's latest high-performance, motor control, C2000™ real-time microcontroller and PMICs which both include on-chip safety functionality. Designers can potentially achieve lower costs of the overall system, associated with a smaller BOM size implementation, and reduce the time-to-market for this solution by using the C2000 product family, these design concepts, and additional TI Functional Safety resources.