SPRAD98A May 2023 – November 2026 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
The ISO 3691-4 standard defines the safety requirements and verifications for driverless industrial trucks, including industrial mobile robots (IMRs), such as autonomous mobile robots (AMRs). The standard describes the safety requirements of the overall machine; however, the designer is responsible for determining where the safety functions are placed within the industrial truck modules, as seen in Figure 2-1.
The ISO 3691-4 safety standard describes the safety considerations that must be implemented to meet necessary risk reductions when a hazardous situation exists. For each of the described risk situations, the ISO 3691-4 standard assigns a minimum required performance level (PL) according to the ISO 13849-1 standard. The PL is a value commonly used to achieve the required risk reduction for each safety function and is defined in the machinery standard of ISO 13849-1 (Section one).
Similar to the PL, several standards use the safety integrity level (SIL) to measure the system safety performance. The parameters of the SILs are defined in the IEC 61508 standard. The relationship between the PL and SIL is found in Table 2-1.
| Hardware Fault Tolerance (HFT) | Category | ||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|
| IEC 61508 | ISO 13849 | ||||||||||
| 0 | 1 | 2 | 0 | 1 | 2 | SFF | DC(1) | 1 | 2 | 3 | 4 |
| - | SIL 1 | SIL 2 | SIL 1 | SIL 2 | SIL 3 | < 60% | None | ||||
| SIL 1 | SIL 2 | SIL 3 | SIL 2 | SIL 3 | SIL 4 | 60% to < 90% | Low | c | c | d | |
| SIL 2 | SIL 3 | SIL 4 | SIL 3 | SIL 4 | SIL 4 | 90% to < 99% | Medium | d | e | ||
| SIL 4 | SIL 4 | SIL 4 | SIL 4 | SIL 4 | ≤ 99% | High | e | ||||
| Type B | Type A | ||||||||||
The SIL and PL both define the safety levels of performance according to the standards used for evaluation (IEC61508 or ISO13849). These levels quantify diagnostic coverage by using different parameters. The SIL uses the safety failure fraction (SFF) as the parameter to quantify the ratio between the safe faults of the system and the total faults of the system. Similarly, the PL refers to the DC parameter as a measure of the effectiveness of the diagnostics implemented in the system. However, DC is the ratio of detected dangerous faults versus all dangerous faults. The SIL and PL are related through two main parameters which are inversely proportional: MTTFd (mean time to dangerous failure)—used in the ISO standards—and PFH (probability of dangerous failure per hour)—used in IEC standards for high demand systems. By using this relationship, using both levels (PL and SIL) is possible when assessing a system for safety.
| PL (ISO 13849) | PFH Target Values [PFH = 1/MTTFd] |
SIL (IEC 61508, IEC 62061) |
|---|---|---|
| a | ≥ 10-5 to < 10-4 | No correspondence |
| b | ≥ 3 x 10-6 to <10-5 | 1 |
| c | ≥ 10-6 to < 3 x 10-6 | 1 |
| d | ≥ 10-7 to < 10-6 | 2 |
| e | ≥ 10-8 to < 10-7 | 3 |
Although the PL or SIL applies to the complete safety function typically formed by sensors, data processing, and actuators, each one of these function subsystems must meet a minimum PL or SIL. For each subsystem, a different standard exists to describe how the safety level is met. As an example, for motor drive and actuator implementations, the specific subsystem standard (IEC 61800-5-2) is used to specify the safety requirements. The IEC 61800-5-2 standard defines the requirements for the design and development of variable speed drives by describing the designated safety subfunctions, for example as safe torque off (STO), safe limited speed (SLS), safe brake control (SBC), and so forth. Within the standard, IEC 61800-5-2 refers to the ISO 13849-1 standard and describes the requirements necessary for each subfunction to achieve a minimum PL. Moreover, aspects such as independence between systems, redundancy, and the processing time are discussed on both previously-mentioned standards and must be considered when implementing the system. Therefore, prior to starting the system implementation, understanding the key relationships between the safety requirements is important for each application, for each safety subfunctions that must be implemented, and for each level of required risk reduction (SIL or PL) for each subfunction. For this specific use-case (as summarized in Table 1 of the ISO 3691-4 standard), a minimum PLd safety level is required. Focusing on the motor drive subsystem, the safety subfunctions defined in the IEC 61800-5-2 standard are used to meet the PLd requirements.
Table 2-3 summarizes the main relationships between the three standards.
| Safety Function per EN ISO 3691-4 |
Minimum Required PL per EN ISO 3691-4 | Related Safety Subfunction per IEC 61800-5-2 |
|---|---|---|
| Breaking System | d/b | SBC, SS1, STO |
| Speed control | d/c | SLS, SOS, STO |
| Automatic Battery Charging | b | NR(1) |
| Load Handling | b | NR(1) |
| Steering | – | SLS |
| Stability | c | NR(1) |
| Emergency Stop Function | d | STO |
| Personnel Detection Systems | d/c | SLS, SOS, SS1, STO SDI |
| Automatic, Manual, and Maintenance Modes | d/c | SLS, SOS, STO |
| Warning Systems | a | NR(1) |
| Access Into the Confined Zone | d | SOS, STO |