SPRADA9C August 2024 – October 2025 AM62P , AM62P-Q1
The partial IO circuits will be disabled the first time power is applied to the processor. When the partial IO circuits are disabled, the MCU_PORz input signal will propagate to these circuits. The MCU_PORz input signal is blocked from these circuits after software enables the partial IO functionality (circuits) and configures the processor to monitor wakeup inputs. This is necessary since the MCU_PORz input signal will be asserted by the PMIC when it begins the power down sequence associated with the other processor power rails.