SPRADT9 August 2026 AWR2188
Waveform configuration for the AWR2188 includes the following steps:
Figure 3-1 below shows the storage locations and associations of each configuration in the RAM.
Figure 3-1 Waveform Configuration Storage Locations and AssociationsAs shown in Figure 3-1, for the waveform generation of each frame, first locate the frame configuration; then locate the corresponding subframe configuration in the chirp RAM based on the h_SubFrameLutOffset setting in the frame configuration; and finally index the profile and TxEnable configurations in the chirp RAM according to the defined chirp LUT configuration to generate the corresponding chirps.
For the AWR2188 waveform configuration, the basic API configuration flow is shown in Figure 3-2 below. The chirp parameter LUTs provide great flexibility for the generation of different waveforms.
Figure 3-2 API Configuration FlowThe following is a detailed description of frame, subframe, chirp parameter LUT, and profile. See also Reference[5] for detailed configuration parameter structures and APIs.