SPRT770 April   2024 AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Acronyms Used in This Document
  6. 3ROM Boot Requirements
  7. 4Application Requirements
  8. 5Additional Usage Factors
  9. 6Flash Support in MCU PLUS SDK
  10. 7Compatible Flash Devices
  11. 8Tested Flash Devices
  12. 9References

ROM Boot Requirements

As Figure 1-2 shows, the boot flow process is a sequence adopted by AM263P that starts upon power-on. ROM code on the R5F is set to work in a certain way which is described in the Initialization chapter of the device-specific Technical Reference Manual. The ROM code expects specific instructions from the flash and expects specific timing and framing configurations for establishing communication. Multiple boot modes are supported in the AM263P device, and ROM code expects the following support:

  • Flash device must operate in the 3.3V vicinity
  • In OSPI boot mode, the flash must support Octal Output Fast Read (opcode 0x8B) and the 1S-1S-8S transfer protocol
  • In QSPI boot mode, the flash must support Quad Output Fast Read (opcode 0x6B) and the 1S-1S-4S transfer protocol
  • Flash device must allow 8 dummy clock cycles for setting up the initial address during the previously-mentioned read operations
  • Flash device must boot in 1S mode by default
  • Flash must support 3-byte (24-bit) addressing mode by default
  • Flash memory size 4MB is recommended as a minimum
  • Due to device errata item i2426, the boot ROM does not support devices that use an extended opcode. This issue only applies to flash memories that need extended opcode support in 8D boot mode. 1S and 8S boot modes are not impacted by this limitation. Support for this feature is planned for future device revisions.

All of this information is available in the data sheet of the flash device being evaluated. A flash device must support all of the points mentioned above to meet AM263P compatibility requirements.