SPRT770 April   2024 AM263P2 , AM263P2-Q1 , AM263P4 , AM263P4-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Acronyms Used in This Document
  6. 3ROM Boot Requirements
  7. 4Application Requirements
  8. 5Additional Usage Factors
  9. 6Flash Support in MCU PLUS SDK
  10. 7Compatible Flash Devices
  11. 8Tested Flash Devices
  12. 9References

Additional Usage Factors

Consider the following items when deciding on what flash part to use for the application:

  • What is the flash required for? Some applications require more flash storage than others depending on whether of not the memory is used for booting or storage.
  • Is the entirety of the memory be used? A smaller and lower-cost flash device can be used if a large storage space is not needed.
  • Is the application heavily flash dependent? Typically, 8MB to 16MB is enough for an application, but this varies depending on how heavily external storage is being used.
  • Does the flash part support a RESET signal? If at any point of the application 4-byte addressing mode must be used, then a RESET signal is required to prevent booting problems upon reset.
  • Flash device with RWW support must be used if this function is intended to be used during application