SPRU514AA July 2001 – March 2026 SM320F28335-EP
The compiler produces relocatable blocks of code and data. These blocks, called sections, are allocated in memory in a variety of ways to conform to a variety of system configurations. See Section 7.1.1 for a complete description of how the compiler uses these sections.
The compiler creates two basic kinds of sections: initialized and uninitialized. Table 4-1 summarizes the initialized sections. Table 4-2 summarizes the uninitialized sections.
| Name | Contents | Restrictions |
|---|---|---|
| .args | Reserved space for copying command line arguments before the main() function is called by the boot routine. See Section 2.6. | |
| .binit | Boot time copy tables (See the Assembly Language Tools User's Guide for information on BINIT in linker command files.) | |
| .c28xabi.exidx | Index table for exception handling; read-only. (EABI only) | Program |
| .c28xabi.extab | Unwinding instructions for exception handling; read-only. (EABI only) | Program |
| .cinit | Tables for explicitly initialized global and static variables. (1) | Program |
| .const | Global and static const variables that are explicitly initialized and contain string literals. String literals are placed in the .const:.string subsection to enable greater link-time placement control. (EABI only) | Data |
| .data | Global and static non-const variables that are explicitly initialized. (1) | Data |
| .econst | Global const variables that are explicitly initialized or contain string literals. String literals are placed in the .econst:.string subsection to enable greater link-time placement control. (COFF only) | Data |
| .init_array | Table of constructors to be called at startup. (EABI only) | Program |
| .ovly | Copy tables other than boot time (.binit) copy tables. | |
| .pinit | Table of constructors to be called at startup. (COFF only) | Program |
| .ppdata | Data tables for compiler-based profiling (see the --gen_profile_info option). | Data |
| .ppinfo | Correlation tables for compiler-based profiling ( see the --gen_profile_info option). | Data |
| .switch | Jump tables for large switch statements. | Program without -unified_memory option Anywhere with -unified_memory option |
| .text | Executable code and constants. | Program |
| Name | Contents | Restrictions |
|---|---|---|
| .bss | Global and static variables (EABI only) | Anywhere in data |
| .ebss | Global and static variables (COFF only) | Anywhere in data |
| .stack | Stack | Low 64K |
| .sysmem | Memory for malloc functions (heap) (EABI only) | Anywhere in data |
| .esysmem | Memory for malloc functions (heap) (COFF only) | Anywhere in data |
When you link your program, you must specify where to allocate the sections in memory. In general, initialized sections are linked into ROM or RAM; uninitialized sections are linked into RAM.
The linker provides MEMORY and SECTIONS directives for allocating sections. For more information about allocating sections into memory, see the TMS320C28x Assembly Language Tools User's Guide.