11 Revision History
Changes from December 15, 2023 to March 15, 2024 (from Revision J (December 2023) to Revision K (March 2024))
- Updated compiler versions with which C7000 Host Emulation was
built.Go
Changes from August 5, 2022 to December 15, 2023 (from Revision I (August 2022) to Revision J (December 2023))
- Corrected example for multiple element swizzle accessor
workaround.Go
- Corrected example code.Go
Changes from October 22, 2021 to August 5, 2022 (from Revision H (October 2021) to Revision I (August 2022))
- Added __C7X_HOSTEM__, __C7120__, and __C7504__ preprocessor
symbols.Go
- Simplified example program syntax since the cl7x compiler now
accepts the constructor-style syntax for vector initialization.Go
- Native vector types are now called "TI vector types." In addition,
several limitations related to complex vector types have been resolved. See the
C7000 C/C++ Optimizing Compiler User's Guide for
details.Go
- Both cl7x and Host Emulation compilers now accept constructor-style syntax
for vector initialization.Go
- Clarified types of accessors supported, and updated workarounds for swizzle
accessors.Go
- Modified example code.Go
- Updated table of key terms found in vector-related errors and
warnings.Go
- Updated table of errors and warnings related to syntax
changes.Go
Changes from March 15, 2021 to October 22, 2021 (from Revision G (March 2021) to Revision H (October 2021))
- Added a list of pointer comparisons operators to vector and complex
element pointer types.Go
Changes from December 31, 2020 to March 15, 2021 (from Revision F (December 2020) to Revision G (March 2021))
- Allow Visual C++ build tools versions after 2017.Go
- Both release and debug-compatible static run-time
libraries are provided for use with Microsoft Visual
C++.Go
- The initial values of control registers are now set to the values
used in a hardware reset instead of setting all control register values to
0.Go
Changes from May 1, 2020 to December 31, 2020 (from Revision E (May 2020) to Revision F (December 2020))
- Updated the numbering format for tables, figures, and
cross-references throughout the document.Go
- Noted that Host Emulation support is an experimental product, and
its limitations should be considered.Go
- Added -fno-strict-aliasing option to command line for g++ compiler.
Corrected error in sample code.Go
- Array access operators are not supported for vector and complex
element pointer types.Go
- The vector ternary operator is not supported with C7000 Host
Emulation.Go
- Modified example code.Go
- Modified example code.Go