SPRUIG8I January 2018 – December 2023
C/C++ source code may need to refer to symbols that are defined by the linker, not in C/C++ source code. For linker-defined symbols that act like a function or array, you can often refer to such symbols in a straightforward way in C/C++ code. For other purposes in C/C++ code, you typically need to use other techniques, such as the _symval operator, to access linker-defined symbols. These techniques are described in the subsections that follow.