SPRUIG8I January 2018 – December 2023
A file can be opened to a user-defined device driver by using a device prefix in the pathname. The device prefix is the device name used in the call to add_device followed by a colon. For example:
FILE *fptr = fopen("mydevice:file1", "r");
int fd = open("mydevice:file2, O_RDONLY, 0);
If no device prefix is used, the HOST device will be used to open the file.