SPRUIY1C November 2020 – April 2024
The connectivity is provided through the micro USB connector over the onboard XDS110 (TM4C1294NCPDT) emulator. This provides the following interfaces to the PC:
When the USB is connected to the PC, the device manager recognizes two XDS110 COM ports under Ports (COM and LPT).
XDS110 debug probe and data port are detected under Texas Instruments Debug Probes.
If the PC is unable to recognize the above COM ports, then install the EMU pack available at the following link:
https://software-dl.ti.com/ccs/esd/documents/xdsdebugprobes/emu_xds_software_package_download.html