SPRUJ27C November 2022 – November 2023 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
Verifies region specified against specified PSA value
Synopsis
Fapi_StatusType Fapi_doPsaVerify(
uint32 *pu32StartAddress,
uint32 u32Length,
uint32 u32PsaValue,
Fapi_FlashStatusWordType *poFlashStatusWord)
Parameters
| pu32StartAddress [in] | start address for region to verify PSA value | |
| u32Length [in] | length of region in 32-bit words to verify PSA value | |
| u32PsaValue [in] | PSA value to compare region against | |
| poFlashStatusWord [out] | returns the status of the operation if result is not Fapi_Status_Success | |
| ->au32StatusWord[3] | Actual PSA |
Description
This function verifies the device against the supplied PSA value starting at the specified address for the length of 32-bit words specified. The calculated PSA value is returned in the poFlashStatusWord parameter.
Restrictions
None
Return Value