SPRUJ27C November 2022 – November 2023 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
Remaps an ECC address to data address and calls Fapi_issueProgrammingCommand().
Synopsis
Fapi_StatusType Fapi_issueProgrammingCommandForEccAddress(
uint32 *pu32StartAddress,
uint16 *pu16EccBuffer,
uint16 u16EccBufferSizeInBytes)
Parameters
| pu32StartAddress [in] | ECC start address in Flash for the ECC to be programmed |
| pu16EccBuffer [in] | pointer to the ECC buffer address |
| u16EccBufferSizeInBytes [in] | number of bytes in the ECC buffer If the number of bytes is 1, LSB (ECC for lower 64 bits) gets programmed. MSB alone cannot be programmed using this function. If the number of bytes is 2, both LSB and MSB bytes of ECC get programmed. |
Description
This function will remap an address in the ECC memory space to the corresponding data address space and then call Fapi_issueProgrammingCommand() to program the supplied ECC data. The same limitations for Fapi_issueProgrammingCommand() using Fapi_EccOnly mode applies to this function. The LSB of pu16EccBuffer corresponds to the lower 64 bits of the main array and the MSB of pu16EccBuffer corresponds to the upper 64 bits of the main array.
Return Value